I have noticed that once the code composer studio vers 6.1.2 is opened on my windows 7 64 bit machine I see cmd.exe and conhost.exe in the Windows Security log. This is having some concern due to the fact that both of those exe's are hitting the log at a rate of twice per second for the entire duration that the studio is opened. Once I close it the logging stops. Is there a configuration or install step that was missed or does it really require this many modifications to the command line? A few hits would be expected but we are talking over 100,000 in an 8 hour shift. Can anyone help or explain this?
Simply clearing the log is not a viable solution in this case.