After performing a fresh installation of CCS 6.1.3.00033 in Linux (CentOS 6.7 64-bit) in which selected to install Blackhawk drivers the following error was reported when I run the install_drivers.sh script:
$ sudo /opt/ti/ti_ccs6_1_3/ccsv6/install_scripts/install_drivers.sh [sudo] password for Mr_Halfword: Uninstalling /etc/udev/rules.d/71-ti-permissions.rules TI XDS100 installation completed successfully. Some versions of Linux require a reboot in order for the driver to function properly. For other versions restarting udev is sufficient. Restarting udev now ... Starting udev: [ OK ] Starting udev: [ OK ] bhERROR: Could not locate CCSv5 INSTALLDIR. Now exiting script... Starting udev: [ OK ]
Not sure why the error is reported about a CCSv5 INSTALLDIR since had installed CCS 6.1.3. I haven't investigated the error, since CCS 6.1.3 is able to use a Blackhawk USB560-M Emulator, 20 pin JTAG. The PC had previously been using earlier versions of CCS 6, so not sure if the error about not locating the CCSv5 INSTALLDIR would cause a problem on a PC which had never had the Blackhawk drivers installed from a previous version of CCS.
The version of Blackhawk Emulators installed in CCS 6.1.3 is 6.0.0.347. I haven't updated to version 6.0.83.001, for the reason described in https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/504702