Tool/software: Code Composer Studio
Hi Everybody,
i have the following code:
if(f_in_motion == TRUE ) { f_p_zero = FALSE; return; }
f_in_motion - signed char
TRUE is define as 1
but when i'm debugging and the f_in_motion is FALSE (0) it also enter the brackets and doesn't continue to further line at the bottom
why the condition is fullfiled?
i've attached an image of the debug process