Tool/software: Code Composer Studio
Many years ago, Robert W posted this question. It was NOT answered:
I have now done the same thing. In the properties, I clicked that RTSC SYS/BIOS and it stuffed a config file in the project. Now I have "unclicked" the box, and removed the CFG file... But it continues to insist that there must be a CFG file. And the associated XDC build will stuff it's code and libraries in there, which I do not want.
This is CCS 7.2
To say that once the CFG file have been accidentally added afterwards, it now has to remain there forever, is essentially saying the IDE has infested the project with a virus that can't be removed. To say that all RTSC projects need a config file does not answer the question of how to make the project back into a NON-RTSC project.
The project was created without RTOS SYS/BIOS, and needs to be set back to that state.
How does one do that?
Buildfile generation error occurred.. This project does not contain a buildable RTSC Configuration (.cfg) file. In order for it to build, this project must contain one RTSC Configuration file that is not excluded from build. Build stopped..
-CSW