Other Parts Discussed in Thread: UNIFLASH, CONTROLSUITE
Tool/software: Code Composer Studio
Hello,
For initial phase of development our project uses TMS320F2808 evaluation board.
To generate the hex file I used below flag settings in CCS 6.0.1.00040.
--fill=0xffff --memwidth=16 --romwidth=16 --intel
But when I try to flash the hex file into the board I get "no source available for 0x0" error.
It all works fine, when I flash the .out file.
Last week I got response from TI to try to reset the chip and restart the program. I did that, but still it is not working.
To make sure that everything is OK with the .cmd file, I used .cmd from example project. The same is attached.
Is there anything that I am missing here?
Best Regards,
Sanat
/* // TI File $Revision: /main/4 $ // Checkin $Date: August 2, 2006 16:57:00 $ //########################################################################### // // FILE: F2808.cmd // // TITLE: Linker Command File For F2808 Device // //########################################################################### // $TI Release: DSP280x C/C++ Header Files V1.70 $ // $Release Date: July 27, 2009 $ //########################################################################### */ /* ====================================================== // For Code Composer Studio V2.2 and later // --------------------------------------- // In addition to this memory linker command file, // add the header linker command file directly to the project. // The header linker command file is required to link the // peripheral structures to the proper locations within // the memory map. // // The header linker files are found in <base>\DSP280x_Headers\cmd // // For BIOS applications add: DSP280x_Headers_BIOS.cmd // For nonBIOS applications add: DSP280x_Headers_nonBIOS.cmd ========================================================= */ /* ====================================================== // For Code Composer Studio prior to V2.2 // -------------------------------------- // 1) Use one of the following -l statements to include the // header linker command file in the project. The header linker // file is required to link the peripheral structures to the proper // locations within the memory map */ /* Uncomment this line to include file only for non-BIOS applications */ /* -l DSP280x_Headers_nonBIOS.cmd */ /* Uncomment this line to include file only for BIOS applications */ /* -l DSP280x_Headers_BIOS.cmd */ /* 2) In your project add the path to <base>\DSP280x_headers\cmd to the library search path under project->build options, linker tab, library search path (-i). /*========================================================= */ /* Define the memory block start/length for the F2808 PAGE 0 will be used to organize program sections PAGE 1 will be used to organize data sections Notes: Memory blocks on F2808 are uniform (ie same physical memory) in both PAGE 0 and PAGE 1. That is the same memory region should not be defined for both PAGE 0 and PAGE 1. Doing so will result in corruption of program and/or data. L0/L1 and H0 memory blocks are mirrored - that is they can be accessed in high memory or low memory. For simplicity only one instance is used in this linker file. Contiguous SARAM memory blocks or flash sectors can be be combined if required to create a larger memory block. */ MEMORY { PAGE 0: /* Program Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */ RAML0 : origin = 0x008000, length = 0x001000 /* on-chip RAM block L0 */ OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */ FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */ FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */ FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */ CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */ CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ ROM : origin = 0x3FF000, length = 0x000FC0 /* Boot ROM */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */ /* Registers remain on PAGE1 */ RAMM0 : origin = 0x000000, length = 0x000400 /* on-chip RAM block M0 */ BOOT_RSVD : origin = 0x000400, length = 0x000080 /* Part of M1, BOOT rom will use this for stack */ RAMM1 : origin = 0x000480, length = 0x000380 /* on-chip RAM block M1 */ RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */ FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */ RAMH0 : origin = 0x3FA000, length = 0x002000 /* on-chip RAM block H0 */ } /* Allocate sections to memory blocks. Note: codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code execution when booting to flash ramfuncs user defined section to store functions that will be copied from Flash into RAM */ SECTIONS { /* Allocate program areas: */ .cinit : > FLASHA PAGE = 0 .pinit : > FLASHA, PAGE = 0 .text : > FLASHA PAGE = 0 codestart : > BEGIN PAGE = 0 ramfuncs : LOAD = FLASHD, RUN = RAML0, LOAD_START(_RamfuncsLoadStart), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), PAGE = 0 csmpasswds : > CSM_PWL PAGE = 0 csm_rsvd : > CSM_RSVD PAGE = 0 /* Allocate uninitalized data sections: */ .stack : > RAMM0 PAGE = 1 .ebss : > RAML1 PAGE = 1 .esysmem : > RAMH0 PAGE = 1 /* Initalized sections go in Flash */ /* For SDFlash to program these, they must be allocated to page 0 */ .econst : > FLASHA PAGE = 0 .switch : > FLASHA PAGE = 0 /* Allocate IQ math areas: */ IQmath : > FLASHC PAGE = 0 /* Math Code */ IQmathTables : > ROM PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */ /* .reset is a standard section used by the compiler. It contains the */ /* the address of the start of _c_int00 for C Code. /* /* When using the boot ROM this section and the CPU vector */ /* table is not needed. Thus the default type is set here to */ /* DSECT */ .reset : > RESET, PAGE = 0, TYPE = DSECT vectors : > VECTORS PAGE = 0, TYPE = DSECT } /* //=========================================================================== // End of file. //=========================================================================== */