Other Parts Discussed in Thread: 66AK2G02
Tool/software: Code Composer Studio
Hi !
I try to built Hello World application for custom board based on 66AK2E05. I use this and this guides.
I use 66AK2G02.lds file with the following corrections:
MSMC_SRAM : o = 0x0C000000, l = 0x00100000 /* 1MB MSMC Shared SRAM */
MSMC_SRAM : o = 0x0C000000, l = 0x00200000 /* 2MB MSMC Shared SRAM */
DDR0 : o = 0x80000000, l = 0x80000000 /* 2GB external DDR0 */
DDR0 : o = 0x80000000, l = 0x40000000 /* 1GB external DDR0 */
When I allocate sections in MSMC_SRAM (in lds file):
} > MSMC_SRAM
the application is executed correctly.
But when I allocate sections to DDR0:
} > DDR0
the application causes an error at startup.
How do I correctly allocate the program in DDR memory?
ССS7.4. Win7 32bit.
DDR Memory is correctly initialized in GEL, ddr_memory_test script passed.