Part Number: EVMK2H
Tool/software: Code Composer Studio
Hello
We are unable to connect the board EVMK2H Rev4.0 through XDS200 with CCS under Ubuntu 16.04
We narrowed the problem to the software release of JTAG xds200 onboard usb adapter on EVMK2H boards :
It is a 1.0.0.2 release ( and the latest is 1.0.0.8 ). We try to update a board following TI instructions with CCSv7.30.00019 :
http://processors.wiki.ti.com/index.php/XDS200#Updating_the_XDS200_firmware
As the xds200 is connected with an external XDS220 and connected to the host, we try to load the last version of the firmware xds200-firmware-v1008.bin obtained from CCV7\ccs_base\uscif\xds200
Message error was displayed as Load Memory Failed Data Verification failed at address 0x80017ff0 (see attached picture)
The distribution CCSV7 only contains am1808.gel
We tried also the procedure with CCSV6.0.1.00040 with the same results
As we checked , all our EVM2KH XDS200 onboard firmware is 1.0.0.2 and are thus unusable on linux for emulation purposes.
Do you have any procedure to make it possible to connect to the board ?
See picture attached
Regards
Clement