Tool/software: Code Composer Studio
Hello,
when I try to use my USB200 I get a message that I should update the firmware. I tried to do so, but I get the following error:
C:\ti\ccs_base\common\uscif\xds2xx>xds2xx_conf.exe get xds2xxu 0
boardRev=2
ipAddress=0.0.0.0
ipConfig=dhcp
ipGateway=255.255.255.255
ipNetmask=255.255.255.255
productClass=XDS2XX
productName=XDS200
serialNum=00:0F:D2:05:06:32
swRev=1.0.0.5
hostCPU=AM1802
emuCtrlType=Bit bang
extMemType=SDRAM
portUSB=true
portENET=false
portWIFI=false
portRS232=false
EnableUSBSerial=true
CurrentMeasure=false
C:\ti\ccs_base\common\uscif\xds2xx>xds2xx_conf.exe update xds2xxu 0 xds200_firmware_v1008.bin
ERROR: failed firmware update
Error : test failed
The error is also there on another computer and also with version 6.0.83.1 of the emulator package.
I also tried different USB ports. There is no target connected.
When I try to update within CCSv7 then I get:
But there is for sure no second probe connected. I verified that by "xds2xx_conf.exe get xds2xxu 1", which cannot find a probe.
What should I do now?
Best regards,
Thomas.