Hi,
I am using dsk6455 and ccs 3.3. Where I can find example of burning some data on dsk6455 flash?
Thank you in advance!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using dsk6455 and ccs 3.3. Where I can find example of burning some data on dsk6455 flash?
Thank you in advance!
Have you checked out SDS's website? There is some documentation there.
http://www.softwaredesignsolutions.com/flashburn.aspx
Thanks
ki
Akash Mullangi said:Is there any way to convert the .out file that i have got (from embedded coder ,simulink) to hex for DSK 6455 ?
Yes. A hex conversion utility comes with the compiler installation. See Chapter 11 of:
http://www.ti.com/lit/ug/spru186v/spru186v.pdf
Thanks
ki
Hi,
If you have a project, there is also a post-build step that is automatically configured. Check this thread.
Regards,
Rafael
Hi,
The post build step can itself runs from the command-line, but because a project is used, all the Eclipse variables are properly resolved: the ${CG_TOOL_HEX}, ${BuildArtifactFileName}, etc. In the case of using an external builder, you will have to create your own post build step by following the syntax required by the utility <tiobj2bin.bat>. I suggest opening this batch file in a text editor as it contains its usage details (I couldn't find it documented anywhere else).
Hope this helps,
Rafael
Hi Again ,
The command say "${CG_TOOL_ROOT}/bin/hex${CG_TOOL_SUFFIX}.exe" --ti_txt "${BuildArtifactFileName}" -o "${BuildArtifactFileBaseName}.txt" -order MS -romwidth 16 .
I have resolved the things you have said ,
But what about the rest of the option like , entry point and stuff ?
dose hex6x utility build with all the defaults ?
PS: Thanx a lot for the support , I really Appreciate it .
Akash
Akash Mullangi said:Hi Again ,
The command say "${CG_TOOL_ROOT}/bin/hex${CG_TOOL_SUFFIX}.exe" --ti_txt "${BuildArtifactFileName}" -o "${BuildArtifactFileBaseName}.txt" -order MS -romwidth 16 .
I have resolved the things you have said ,
But what about the rest of the option like , entry point and stuff ?
dose hex6x utility build with all the defaults ?
As I mentioned earlier, please read Chapter 11 of:
http://www.ti.com/lit/ug/spru186v/spru186v.pdf
It has all the details of the hex utility
Thanks
ki
Hi Ki ,Rafael,
How do i remove the offset ? using the utility ...?
Do I have to use the memory image option ?
Akash,
Flashburn is not a product from TI. Please visit the SDS site for more information on Flashburn.
http://www.softwaredesignsolutions.com/flashburn.aspx
Thanks
ki
Hi ki ,
Could you help me with this , I am not able to input the option to the hex6x utility file ...
The command that I used is : hex6x -a L1_Wavlet.out -memwidth 8 -image ROMS { FLASH : org = 0xB0000000, len = 0x2000, romwidth = 8, files = {OM2.hex} }
Is there anything wrong in the order of the inputs ?
one last help ki ... I think ill be done :)
Thank you
Hi ki ,
Could you help me with this , I am not able to input the option to the hex6x utility file ...
The command that I used is : hex6x -a L1_Wavlet.out -memwidth 8 -image ROMS { FLASH : org = 0xB0000000, len = 0x2000, romwidth = 8, files = {OM2.hex} }
Is there anything wrong in the order of the inputs ?
one last help ki ... I think ill be done :)
Thank you
Akash Mullangi said:The command that I used is : hex6x -a L1_Wavlet.out -memwidth 8 -image ROMS { FLASH : org = 0xB0000000, len = 0x2000, romwidth = 8, files = {OM2.hex} }
Is there anything wrong in the order of the inputs ?
The ROMS directive is not an option that can be specified on the command line. It needs to be inside a hex command file which is then passed as an option to hex6x. Please refer to the hex conversion utility details in the C6000 Assembly Language Tools Users Guide.
hi Aarti ,
I did try that in the first case with these parameters .
/*******************************************************************************
* Copyright 2004-2005 - Software Design Solutions, Inc. All rights reserved.
*
* Portions of this work have been provided under license with Texas
* Instruments Inc.
*
* $RCSfile: BlinkDSK6455_hex.cmd,v $
* $Revision: 1.1 $
*
* Creates an ASCII Hex formatted .hex file.
*
******************************************************************************/
L1_Wavlet.out
-a
-memwidth 8
-image
ROMS
{
FLASH: org = 0xB0000000, len = 0x2000, romwidth = 8, files = {"C:\Users\Sahil\Desktop\OM2.hex"}
}
pause
but it says invalid input ....
I did try this cmd line :
cd C:\ti\ccsv5\tools\compiler\c6000\bin
hex6x --ascii "C:\Users\Sahil\Documents\AHM Target Models\L1_Wavlet_ticcs\L1_Wavlet.out" -o "C:\Users\Sahil\Desktop\OM1.hex" -order L -romwidth 8
pause
I was able to generate the hex file.
Just that I was not able input the ROM options ......
Akash Mullangi said:but it says invalid input ....
What is the exact error? I created a similar looking hex.cmd file (I removed the pause at the end) and was able to use it succesfully without errors. I simply run it as:
hex6x hex.cmd