Part Number: TCI6630K2L
Tool/software: Code Composer Studio
Hello,
I have a customer running into the following issue. Can you please advice? Thank you,
I have a project that I can currently build with the following build settings (shown in image), but I would like to upgrade the BIOS from the DSP BIOS to the latest SYS BIOS as well as change the output format to EABI in order to run on a TCI6630K2L Target (TMS320C66x DSP). I am trying to follow the documentation (Migrating a DSP/BIOS 5 Application to SYS/BIOS 6) to convert a DSP BIOS project to use the SYS BIOS. The first task is to convert the config file (projectname.tcf) to a RTSC configuration script. There is supposed to be a tool within XDCTools that allows one to do this (xs, using ti.bios.conversion package within the BOIS install), but the documentation seems to be outdated, since the ti.bois.conversion package has not been part of the BIOS packages since version 6.21.03.21. I tried running with that version, but I’m either calling it wrong or it’s missing dependencies, as I get the following error
js: "C:/Program Files/Texas Instruments/bios_6_21_03_21/packages/ti/bios/conversion/Main.xs", line 31: Error: ti.bios.conversion: TypeError: Cannot call property oldLoadPlat in object [object Object]. It is not a function, it is "undefined".
Is this still the currently prescribed way to convert a DSP BIOS project to a project using SYS BIOS? (using the conversion tool included within BIOS v6.21?)
If so, were could I find help in debugging the conversion tool?
Regards,
Ryan B.