Normal 0 21 false false false MicrosoftInternetExplorer4
Good morning,
I need your help in the following case please:
It is my first project with µC
I’m using your software CSS4. I have no evaluation Kit as Stellaris
® LM3S8962 Ethernet and CAN Evaluation Kit
I’ve installed the software (StellarisWare® Package) .
From step 4(in the QUICKSTART – CODE
COMPOSER STUDIO™ document) and further I receive a “Managed Make Project File Error” which says
“The Managed Make project file could not be read because of the following error:
Error loading Make project information for project driverlib. The tool definition used to create are not available.
Managed Make functionality will not be available for this project.”
What is this tool (red in the massage)?
Can I virtually simulate (without evaluation Kit) the LM3S8938?
Normal 0 21 false false false MicrosoftInternetExplorer4
Best regards
Bassel Daou