Part Number: AM62A7-Q1
I have successfully compiled a neural network model with TIDL. Now I want to run it on the processor using GStreamer, but I want to implement my own custom postprocessing. How do I implement this?
Part Number: AM62P-Q1
Continuous Data Streaming over UART is a use-case across different applications. Lets check the implementation and any additional pointers to take care of while implementing this.
This FAQ applies to other SoCs as well like AM62x…
Part Number: AM263P4 Other Parts Discussed in Thread: SYSCONFIG
What is the meaning of I2C Own Target address in the syscfg file below. Is this related to the I2C controller or the I2C transmitter? What are the valid values it can take?
Part Number: TDA4VH-Q1
TIDL checks for the network version in the model to ensure compatibility with the tidl tools used to compile the model and the C7x firmware running in hardware. This will also be used to check the C7x firmware version that is…
Part Number: TDA4VL-Q1
What are the different callback functions in the ECC test framework in SDL?
What is SDL_ECC_ESMCallBackFunction and when is it called?
What is SDL_ESM_applicationCallbackFunction and when is it called?
What is SDL_ECC_applicationCallbackFunction…
Part Number: AM2634-Q1
LWIP enabled devices can get IP address from DHCP server based on host name. To enable this feature on LWIP stack, certain configuration needs to be done.
- Let us pick the enet_cpsw_tcpserver example to enable this feature…
Part Number: AM263P4
Ethernet packets can be blocked or forwarded based on their packet addresses. Unicast address is a specific type of address that is intended for one to one communication.
ALE in CPSW susbystem can be configured to drop packets…
Part Number: AM2634-Q1 Other Parts Discussed in Thread: SYSCONFIG , UNIFLASH
This FAQ highlights how you make a datastructure to be stored in flash in AM263 microcontroller.
Typically we can do this in AM263Px and AM261x microcontroller where XIP…
Part Number: AM263P4-Q1 Other Parts Discussed in Thread: UNIFLASH
This FAQ explains how to setup the flash utility to flash into external flashes which are not supported out of the box. The method mentioned in this FAQ would be the same for AM261 and…