7824.enc28j60.pp.rar
Hi all,
I got this error when build my project:
**** Build of configuration Debug for project uip_test_msp430f5638 ****
"c:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../ethernet/enc28j60.c'
'Invoking: MSP430 Compiler'
"c:/ti/ccsv6/tools/compiler/msp430_4.3.4/bin/cl430" -vmspx --abi=eabi --data_model=restricted --include_path="c:/ti/ccsv6/ccs_base/msp430/include" --include_path="C:/Users/Tra Quang Kieu/workspace_v6_0/uip_test_msp430f5638/uip/uip" --include_path="C:/Users/Tra Quang Kieu/workspace_v6_0/uip_test_msp430f5638/ethernet" --include_path="C:/Users/Tra Quang Kieu/workspace_v6_0/uip_test_msp430f5638" --include_path="C:/Users/Tra Quang Kieu/workspace_v6_0/uip_test_msp430f5638/uip/apps/dhcpc" --include_path="c:/ti/ccsv6/tools/compiler/msp430_4.3.4/include" --include_path="C:/Users/Tra Quang Kieu/workspace_v6_0/uip_test_msp430f5638/MSP430F5xx_6xx" --advice:power="all" -g --define=__MSP430F5638__ --diag_warning=225 --display_error_number --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=full --preproc_with_compile --preproc_dependency="ethernet/enc28j60.pp" --obj_directory="ethernet" "../ethernet/enc28j60.c"
"../ethernet/enc28j60.c", line 117: remark #1528-D: (ULP 3.1) Detected flag polling using MISTAT_BUSY. Recommend using an interrupt combined with enter LPMx and ISR
INTERNAL ERROR: c:\ti\ccsv6\tools\compiler\msp430_4.3.4\bin\acpia430.exe experienced a segmentation fault
while processing function (unknown or file scope) file ../ethernet/enc28j60.c line 120
This is caused by a defect in the compiler itself. TI Customer
Support may be able to suggest a workaround to avoid this.
Upgrading to the newest version of the compiler may fix this problem.
>> Compilation failure
Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue". Include this ENTIRE error message and a
copy of the .pp file created when option --preproc_with_comment
(-ppc) is used.
gmake: *** [ethernet/enc28j60.obj] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
My project is written in c language. MSP430 compiler version: TI v4.3.4
Can anyone help me.
Thanks.