I use the followling option configuration to compile my for loop statement.
Cl6x -o2 -mf5 -k -mv=6748 --compile_only Continue.cpp
When I analyse the asm file generated by the DSP compiler, I found ILC is used as followlings:
[!A0] BNOP .S1 $C$L4,4 ; |9|
|| [ A0] MVC .S2 B4,ILC
[ A0] MV .L2X A0,B7 ; BRANCHCC OCCURS {$C$L4} ; |9| ;*----------------------------------------------------------------------------* ;* SOFTWARE PIPELINE INFORMATION ;*
I can not find any description of ILC for C6748 in spru733, but find it in spru732. So I doubt whether is some wrong with my complie command. I just want to kown if ILC is exits in C6748.
Thanks