Tool/software: TI C/C++ Compiler
My project is a static library in CCS. To test changes made in the library I have to rebuild my test executable which takes around 20 seconds. Is there a way to have my library relinked with the executable without a full rebuild? Right now when I make a change in the library I build it then I have to rebuild the executable. This is expected as the library gets compiled into the executable but is there a way to speed this up?