Tool/software: TI C/C++ Compiler
Hello.
Today I installed the new version of TI's compiler for ARM and I got the following message error that before wasn't present::
<Linking>
error: symbol "vsnprintf" redeclared with incompatible type:
"int [ExplSign](unsigned char *, size_t, const unsigned char *, va_list)"
in "vsnprintf.c" at line 71 and:
"int [ExplSign](unsigned char *, size_t, const unsigned char *, va_list)"
in
"/home/gtbldadm/processor-sdk-rtos-morty-build/build-CORTEX_1/arago-tmp-exte
rnal-linaro-toolchain/sysroots/x86_64-linux/usr/share/ti/ti-cgt-arm/include/
stdio.h" at line 267)
fatal error #10192: Failed linktime optimization
gmake[1]: *** [M4_ASampleProj.out] Error 1
gmake: *** [all] Error 2
The same code is compiled and linked by the previous version of the compiler v17.9.0 STS.
Best regards,
Scianni Vincenzo