Tool/software: TI C/C++ Compiler
Hi,
We are currently using arm compiler version "ti-cgt-arm_16.9.2.LTS" for the development of AUTOSAR MCAL drivers.
Currently this compiler supports AUTOSAR 3.1 version. We are developing drivers for AUTOSAR 4.2.1 version and the standard types to be defined should be compliant to this.
For example It says for a symbol definition as below.
E_OK, E_NOT_OK
[SWS_Std_00006] ⌈ Name: E_OK, E_NOT_OK Type:
Enumeration Range: E_OK 0x00u E_NOT_OK 0x01u
but in our compiler Std_types.h file it is defined as below, there is no suffix U
#ifndef STATUSTYPEDEFINED
#define STATUSTYPEDEFINED
#define E_OK 0x00
typedef unsigned char StatusType;
#endif
#define E_NOT_OK 0x01.
So please let us know if any new compiler available which supports AUTOSAR 4.2.1 version?