This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to program the DDR3 registers in a TMS320C6671. I'm looking for the sprabl2.zip mentioned in the SPRABL2A.pdf. I have searched TI's website and the link provide is broken. FYI the link is...
http://www.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=sprabl2&fileType=zip
Does anyone know where I can find this file?
I found it myself...by guessing the URL pattern...very sad :(
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=SPRABL2A&fileType=zip
You can click on "Read Abstract" next to "KeyStone DDR3 Initialization (Rev. A)" document to open the following link:
The ZIP file could be downloaded on that page below "Associated Files".
Hi,
Is there an update to the sprabl2.zip files to support 4Gbit DDR3 running at 1600M?
I'm using 4, 16-bit wide, 4Gbit DDR3s to implement a 64-bit DDR3 interface on the TMS320C6678.
Thanks,
Noam
Hi Noam,
As per usage note 14 in the C6678 errata document, the DDR3 interface is limited to a maximum transfer rate of 1333 MT/s.
Regards, Bill
Hi SimonPack,
We're working to get the link fixed. Until then, you can down load the spreadsheet from here.
Regards,
Bill