Hi,
I am not too familiar with TINA, so a little help would be gratefully received.
I have a simple V / I plot representing an output transistor with a protection circuit.
Essentially I have a Voltage controlled current source from a current source controlled by a transistor and a voltage source (0 to 70V DC (VG1)). The VCCS dumps current into a 0.22 Ohm resistor (R1). there is feedback to the transistor from here.
That shows the kind of curve I would expect.
The thing I need to do is add a constant current line at I = 17A and also I = 6.25A from V = 0 to 70. In addition I want to add a constant power dissipation curve for P= 250W from V=10 to 70.
In the post processor I cannot access the X/Y function, it just says " XY plot only allowed in trans or DC mode" which I seem to be in anyway.
I wrote a function for the power copied below but I get " Error in line 5" message when I try to create the function
{This is a template}
{Don't modify the functionname}
Function F(s);
Begin
{Your expressions here}
V1:=V_VG1[5,0];
{The result value}
F := 250/V1;
End;
Is this a syntax thing or is it not possible to do this in TINA?