Trying to format a plot in Webench
Electrical Simulations -> Waveform Controls -> Plot Boundaries
Bode simulation
Setting X-axis, Lower and Upper, then Replot
Result:
Setting lower to 20, the plot starts at 100
Setting lower to 100, the plot starts at 1e3
Expected:
Plot start at 20 and 100Hz respectively
Also trying to set the upper and lower for Y-axis range is completely messed up (basically not obeying the user input)
I guess this might be a bug in the code where the input expected is a real number, but the graph plots in LOG10, upon a Get request from the graph object, the number is not converted back to non-logarhythmic
Latest version of Flash (19.something)