How can I design a symmetrical (±12 V) smps with Webench?
I don't see any option for symmetrical smps.
Can I do it in Webench?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The closest we have would be a 2-Output Flyback with the LM258x. You can do this while in WEBENCH by clicking the new button and then putting 12V out in the Vout 1 box and -12 Vout in the Vout2 box.
Best regards,
Tommy
In WEBENCH I clicked the new button.
I put 12V out in the Vout 1 box
and -12V out in the Vout2 box.
I clicked 'show all recommended Power Management ICs".
I clicked "compare all part types".
Result: Solution found 3:
LM5023
UCC28710
UCC28711
LM258x does not appear in the solutions.
I click on LM5023 "Open Design" and shows me a design with one output only, the +12V.
My apologies,
I did not realize you were doing an AC/DC design. The LM258x series is only enabled for DC/DC conversions. We are really just starting to enable our lineup of AC/DC parts in WEBENCH and have not yet done any multi-output topologies.
You may want to look at some reference designs for what you are doing and possibly some app notes.
A couple good places to start are listed below:
90V to 270V AC Input, -12V to +12V/3W Quasi-Resonant Flyback(12V @ 250mA):
http://www.ti.com/tool/pmp7263.1
Improving Cross Regulation of Multiple Output Flyback Converters:
http://www.ti.com/lit/an/snva562/snva562.pdf
Hope this helps