This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yusuke,
This is Jason and system engineer for TPS65261.
TPS65261 can support VOUT 8V.
Most of customer use TPS65261 for Vout <5.5V, so this "webench" support VOUT <=5.5V for simulation/estimation.
Please send the schematic to me for reviewing.
Hi Jason,
|
Efficiency
Buck1
|
Efficiency
Buck2
|
Efficiency
Buck3
|
Die temperature
|
VIN 10V
|
95%
|
80%
|
94%
|
71 deg
|
VIN 17V
|
94%
|
77%
|
93%
|
77 deg
|
Hi Jason,
Please see my input:
Fsw 600khz
Room Temperature: 25 deg
|
Efficiency Buck1 |
Efficiency Buck2 |
Efficiency Buck3 |
Die temperature |
VIN 10V |
95% |
80% |
94% |
71 deg |
VIN 17V |
94% |
77% |
93% |
77 deg |
Jason Wang
Hi Jason,
Hi Jason,
hi Kiss,
yes, TPS65261 can support Vout 10V when Vin is 12V.
Please share the schematic to me for check when completes.
Jason Wang
jason.wang@ti.com
Dear Jason,
Thank you for your help. I'll send you the schematic, when it's completed.
All the best,
Balazs