hi,
15-28 VDC input and output 100 VDC with 0.1 A circuit i am getting in WEBENCH only i export simulation in to the TINA with same circuit. But, i get only 40V output. so i want same 100 V output for that what should i do.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I get the same results. I can see the circuit is not switching. I'll move your post to the modeling forum
Note:
Customer input the above parameters to webench. Webench exports the included TSC file. The TSC file does not seem to work properly in TINA-TI. Can you tell what is wrong?
I have found that the TINA-TI simulation will run correctly if you simulate for 60ms instead of the 6ms default. This simulation will take longer than the 8 minute cutoff for WEBENCH®. Switching does not start until after about 20ms. If you run the simulation in WEBENCH®, you will also see that the startup simulation only runs for 6ms and does not get to the point of switching.
The WEBENCH® steady state and load/line transient simulations function correctly as well.
ya i got it simulation. now i have one more doubt. i want to make output 100VDC split into positive and negative half of that. i tried with negative voltage converter TL7660 but it can support only 10V is there any alternate.
Well, now we are into another topic. Can you post your actual requirements in a new thread? You may want to post in both isolated and non-isolated forums. Lets see if we can find the proper solution.