Hi,
One of our customer tries to simulate TPS563201 on Webench for 5V Vout condition and find that it could not generate design since the warning of too high junction temperature. From our datasheet, it indeed could support 5V Vout application without a problem. My question here is that is Webench simulation only based on limited number of reference design so not all the working condition can be supported? And our customer also hope to get the stability simulation like bode plot, but I also did not find for TPS563201. Is the bode plot function only applied to limited parts?
Best,
Anthony