Tool/software: WEBENCH® Design Tools
Hi,
Webench parameters:- Vin(min)-10V Vin(max)-14V Vout 24.5V Iout 0.37A (370mA) TPS55340 at 562.300KHz 47uH 96%
Q1: Webench always puts an electrolytic capacitor for the input capacitor, but the data sheet recommends ceramic. When I try to change the component the alternative parts list only shows more electrolytic capacitors. I can't change it for a ceramic. Why? Is it safe to ignore this and just put a ceramic in my actual design.
Q2: Does Webench account for DC bias derating on its output caps? In the above design Webbench uses a 10uf in 0805 package. This cap will probably only give 2uf at output voltage of 24.5V. The data sheet warns to account for DC bias when selecting Cout, but It doesn't appear that Webench does. Is Webench accounting for DC bias when it calculates Rcomp and Ccomp, or is it calculated using 10uf?
Q3: The data sheet recommends to include a 100uf bulk input capacior if the supply is more than a few inches away from the IC. My application is battery powered, from a large-ish 7AH 12V battery through 1 meter of 24AWG cable. The boost converter powers 7 LEDs in series, with very infrequent load changes. Can I dispense with the recommended 100uf bulk input capacitance? I was thinking of increasing the recommended 4.7uf ceramic input to a 10uf 1206 35V and leaving the 100uf ali cap off the board. Anyone have experience with this kind of battery application?
Cheers.