Hi,
The customer is considering use under the following conditions.
VIN = 19 V, Vout = 5 V, Iout = 6 to 8 A, slew rate = 8 to 10 A / μs
When simulating with Webench, there is no problem when default rise time and fall time = 25 μA, but it was not able to normally control at slew rate 9 A / μs. Even if adding an output capacitor was not enough, can you say that this speed response can not follow?
Please let me know the conditions if you can.
TPA53319_rise and fall slew rate=25u.pdf
TPS53319_rise and fall slew rate=1u.pdf
TPS53319_rise and fall slew rate=1u_Cout=1000uF.pdf
Best Regards,
Yuto Sakai