Other Parts Discussed in Thread: DLP3010
I would like to use a DLP device for experiments with digital holography (shaping a laser beam with the DMD, using the HDMI input connected to a computer video card). For this, I need to remove the light engine safely in order to access the DMD directly. I know that this is possible for the DLPLIGHTCRAFTER, there is even an instruction vide on this on Youtube. However, the DLPDLCR3010EVM-G2 device offers more than twice as many pixels for just a bit higher price, so I would prefer that one. Therefore I would like to ask if DLPDLCR3010EVM-G2 is suitable for my purpose. If not, could you please recommend some other DLP device that would be suitable and would have more pixels than the DLPLIGHTCRAFTER?
Thank you very much,
Tomas