This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DLPLCR4500EVM: Blue LEDs stopped working

Prodigy 110 points

Replies: 15

Views: 1037

Part Number: DLPLCR4500EVM

Hi - 

I have been using a DLPLCR4500EVM for a couple of months.  Today when I powered it on, it stopped producing any blue light.  I confirmed with the DLP LightCrafter 4500 Control Software by changing the LED Selection to manual and trying the Red, Green and Blue LEDs only.  The projector is mounted and didn't move between last good operation and today so I don't think anything physical was changed.  

Is there anything I should look at to get the blue led back on?

Thanks,Jeff

  • Hi Jeff,

    Thanks for contacting us in regards your concern on your EVM...
    If I understand your approach correctly, you did put it in Manual mode and enabled the Blue LED only, isn't it? Can you confirm if this worked and what is the LED current reading?

    Below are a couple of troubleshooting activities to understand the signature:
    - Try an internal TPG pattern with a solid field color as red, then as green, and lastly as blue.
    - Flash the system with the original firmware to confirm settings are back to default on the system, then confirm if blue LED comes back ON.
    - Try scoping the blue LED input using a voltmeter to determine if we see anything abnormal.

    Please check with us on any findings to continue exploring this event.

    Thanks and Regards,

    Mario Rodriguez

  • In reply to mario-rm:

    Thanks for the quick response!

    Yes, that's correct. I put it in Manual mode with only the Blue LED enabled. That's when I get no light output.

    The LED current is red=104, green=135, blue=130.

    1. With the "color bars" internal test pattern and manual LED selection set to Red. I get red bars. With Green, I get Green bars. With Blue, I get no light output.
    2. Re-flashed DLPR350PROM_v3.1.0.bin --- Same results.
    3. Blue LED Input voltage --- Sorry, can you tell me specifically what test point or pins I should probe for voltage?

    Thanks
    Jeff
  • In reply to Jeff Youel:

    Hi Jeff,

    No problem... I can explain.

    Under TI Designs, you will find the schematic for such board. Here is a link as a reference: www.ti.com/.../tidr157a.pdf
    By looking at it, it seems like TP64 would be the one you need to check voltage on. Since we know green LED is working, try comparing TP59 (Green Anode) to TP64 (Blue Anode).

    Please let me know if any findings in here.

    Thanks and Regards,

    Mario Rodriguez

  • In reply to mario-rm:

    TP59 = 3.1 V
    TP64 = 29 mV

    Thanks,
    Jeff
  • In reply to Jeff Youel:

    I think we have confirmed we have some sort of strange response from the hardware. We might need to decouple a little bit more.

    Some extra questions below:
    - Do you have an OScope handy to capture a waveform out of TP66 and TP67? We want to understand if the LED is getting enabled properly.
    - In regards the actual blue cathode and anode, can you measure these two (TP64 to TP65), and TP65 to GND as well? This will tell us some more about the LED integrity. As comparison you can use the similar testpoints for a working LED.
    - A little less technical, but valuable information for us: Can you comment in regards the storage conditions for this system (Estimated temperature and humidity)? You mentioned "...the projector did not move between last good operation and today...". Do you know if this was one year from now? Two weeks from now?

    Thanks and Regards,

    Mario Rodriguez

  • In reply to mario-rm:

    Hi -

    1. Sorry, I don't have a scope available right now.
    2a. TP64 - TP65 = 22 mV
    2b. TP65 - GND = 0.9 mV
    3. I've had this projector since April 2018. Its mostly been in my office ~70-80F, nothing unusually with the humidity. Last good operation was Monday of this week. No movement between Mon (Good) and Wed (Failure).

    Thanks
    Jeff
  • In reply to Jeff Youel:

    Is it warm near/close to the blue LED compared to the region near the working LEDs?

    Thanks and Regards,

    Mario Rodriguez

  • In reply to mario-rm:

    No, nothing remarkable, the temperature is pretty consistent across the parts. If there is a specific part that you'd like me to get the temperature from, please let me know, I have an IR thermometer.
  • In reply to Jeff Youel:

    Hi Jeff,

    Thanks for your last inputs...
    We are getting close to determining the root cause. As a follow up with your data, I did some analysis on my end to understand the suspected signature on your blue LED.
    - On my end, any good system is highlighting a max of 2.3~2.5V at TP64, while your system is only outputting 29mV.
    - Enable signal for Blue LED (TP66) should be highlighting an output similar to a square wave when probed using projection (Blue LED projection if set manual Blue only should be constant ~2.9V). It will be helpful to get this pin probed if you can get a hand to an OScope. This should answer to us if we perceive any problems with the LED driver on your system.
    - Temperature will be good to capture on U47 and U46. These parts are located at the backside of the board when looking at the LCR4500EVM top down. I collected temp data after 10min continuous operation, and both are comparable on our good system.
    - One last item would be a continuity test at the blue cable (From the LED input port to J33).

    Please let me know if any inputs on any of these.

    Thanks and Regards,

    Mario Rodriguez

  • In reply to mario-rm:

    Hi Jeff,

    Have you able to solve the problem with your blue LED? If so, I'll temporarily close this thread; but feel free to let us know if we can provide any further assistance here.

    Thanks and Regards,

    Mario Rodriguez

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.