Other Parts Discussed in Thread: DLPC3433, DLPA3000, DLPDLCR2000EVM
I have a DLPDLCR3010EVM with me I want to use only the optical engine and the DLP board I dont want to use the EVM board can I power the Optical engine & DLP board together seperately removing the EVM board connections? and use the device ? in such a case how do I run or attach the DLP board with RGB LED Connectors only to a different system say for now my ubuntu PC ? is there a DLP Lightcrafter display board connector available in market to connect to a different device out put say a different embedded system board? in such a case how do I test the connections and software is available to run and check and then further program on the new embedded system to display the out put I want ?
We are putting together a projector with a embedded system and need help on this?
KIndly let me know
Thanks
Radheevar