Other Parts Discussed in Thread: DLPC350, DLP3010EVM-LC
Hello,
I have a issue that the projector stutter at 120 Hz in the video mode.
I add custom resolutions and 120Hz/ 60Hz refresh rates using intel display settings in Windows 10 and I have tried:
1) Lowering resolution from 1280x800 to 800x600 or 912 x 1140.
2) Using the projector without secondary display which has 60 Hz refresh rates.
3) Lowering 24 BITS to 8 BITS Parallel RGB using GUI.
These methods didn't work well.
Could you suggest me any other solutions to solve this issues?
Thank you.