Hello,
I'm trying to use a Lightcrafter to display simple colored patterns. RGB signals are sent from a PC to the mini-HDMI port. The issue is that all such signals come out of the DLP entirely in grayscale.
The device is still capable of showing full-color patterns. In the GUI, if I set the Video Mode input to the "Color Bar" internal test pattern, and set the LED control to "Automatic", colors display normally. However, if I set the Video Mode input to "Parallel RGB", all inputs result in grayscale outputs. It might be worth noting that I can force the Color Bar pattern to display in grayscale, by changing the LED control to "Manual". This might not be diagnostically relevant, but it's not clear to me why this should happen.
Any advice or guidance would be appreciated!
Notes:
-Issue persists across multiple DLP4500 Lightcrafter devices
-Issue persists across multiple HDMI - mini-HDMI cables
Specs:
OS: Windows 10 Home, 64-bit
Graphics card: GeForce GTX 1060 3GB
GUI: v3.1.0