I am using DLP3000 HDMI mode to display image. The native 608 * 684 input resolution pattern has a one-to-one association with the corresponding micromirror on the DLP 3000. But when I upload a 608*684 pattern to the DLP, the pattern is stretched, i.e. a circle will become ellipse. I searched through the forum and found this thread : https://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/advanced_light_control/f/850/t/170877#pi239031349=1
I know that DLP uses diamond pixel configuration but I am still confused how it stretch the image. The center to center distance of between adjacent pixels should also be equal, which means if I upload a 4*4 square, the appearance on the DLP should also be square.
I noticed that the DLP3000 support 864*480, the aspect ratio is similar to what I saw on the DLP. I wonder how 608*684 mirror array produces 864*480 resolution image.
Thanks!
Ruonan