Hi,
Please tell us the recommended cooling system for DLP 9500 and DLP 7000.
Where is the information on the datasheet?
Especially I heard that using air cooling system is out of warranty.
Best Regards,
Leonardo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please tell us the recommended cooling system for DLP 9500 and DLP 7000.
Where is the information on the datasheet?
Especially I heard that using air cooling system is out of warranty.
Best Regards,
Leonardo
Hello Leonardo,
This information is not in the data sheet because each system implementation is unique and can have very different requirements for fitment and illumination.
What is in the data sheet is information on where to make temperature measurement and calculations to determine the array temperature of the DMD during operation.
There is nothing that precludes the use of air cooling if the heat solution can keep the operational array temperature within specifications.
In many cases where high fluence illumination is used, air cooling systems are unable to remove heat fast enough. In such cases, in order to operate within the Recommended Operating Conditions array temperature specification a liquid cooled solution will likely be required.
It is all about the array temperature.
Best regards,
Fizix
Hi Fizix
Thank you so much for your confirmation.
In the case of DLP9500, the operational array temperature within specifications is 20 to 45 ℃?
Best regards,
Leonardo