Hi,
I input the video signal at 912 x 1140 @ 72 Hz into the HDMI of LCr4500.
The setting conditions are as shown in Figure 1.
Firure 1.
The video source is a combination of a desktop PC and a graphics card.
As shown in Fig. 2, the video information on the GUI is recognized at 912 x 1140 @ 72 Hz. When observing the projection, it is projected at almost 72Hz every frame.
Figure 2.
When I changed the video source to raspberry pi 3, as shown in Fig. 3, the interval between the projected frames became wrong. What is wrong?
For reference, we show the video settings of raspberry pi 3.
Figure 3.
Raspberry Pi 3 video setteings
framebuffer_depth=24
hdmi_force_hotplug=1
config_hdmi_boost=4
hdmi_cvt=912 1140 72 1 0 0 0
hdmi_group=2
hdmi_mode=87
hdmi_drive=2
Best regards,
Masa