Hello, we are looking to incorporate LightCrafter 4500 in our setup for the purpose of 3D modeling using structured light.
We do however need a high depth of focus since we do not want to add any mechanical parts such as a motor to readjust the focus each time.
We found that EKB Technologies has a Laser based system called IR E4500 MKII on their website which as we understand would produce much greater depth of focus, this looks good but we need to work in RGB and not IR.
I couldn't find anything similar in visible range, Is there any solution offered that can support our requirement?
Our capturing distance range is between 65cm to about 1.2 meter.