We have been working with the LightCrafter 4500 which was successfully implemented in our first test setup in R, G, B.
We are now focusing on a parallel setup assembly on a separate bench in which we need specific wavelengths to work with within the UV spectrum at 370-380nm,
Green 520nm and Blue 460-470nm and a requirement in another 3rd test setup in which specifically 590nm range is required.
Is it possible to custom order the LightCrafer 4500 with our wavelength needed combination?