Part Number: DLPLCR6500EVM
Hello,
My name is Nik and I have a Vialux Star-065 projector, it is a 1080p projector with the DLP6500 chipset. I want to make the projected picture smaller but I don't exactly understand how "Display Dimensions" in "video mode" tab work. If I understand correctly "Start Pixel" and "Start Line" are only for positioning the projected picture. The question I really have is what happens whit pixels when I change the values in red boxes (look at the picture below) to a smaller value (e.g. 1920 to 1280 and 1080 to 720). The picture gets smaller indeed but do the pixels get smaller and the resolution of smaller picture is still 1920x1080 or do the non used pixels just shutdown.
I am using projector for 3D SLA printing and pixel size is quite important.
Kind regards, Nik