We're having an issue on one of our pcb's which design is based on the lightcrafter 4500 eval kit design. When the board is cooled below 15-16 degrees C and power is applied, the DLPC350 asserts the Fault Status signal and doesn't boot up to normal operation.
When the board gets back to room temperature, the board again is fully functional and works fine. Some times the heart-beat LED is lit as well as fault status, some times not. All supply voltages and power good-signal etc. are OK. The next step which we haven't tried yet is selectively cooling parts of the board.
Questions:
1. Anyone seen this issue before? Any tips on how we should proceed to debug the issue?
2. What kind of fault conditions does the DLPC350 firmware check before asserting the fault-status flag?