Other Parts Discussed in Thread: DLP4500
Hi all,
I am interested in using a DMD for shaping a fs-laser beam in the NIR range (800nm). I am thinking to make use of the DLP4500NIR.
1. The main issue is related to the maximum power the DMD can resist: the average power hitting the surface will be around 500mW, but the pulses are very short in time (180fs) and a rate of 0.5kHz. The consequent fluence is so about 1mJ per pulse, resulting in very high peak power (MW). I already had problems due to heating with a DLP3000 in these conditions, so I wanted to ask if I can expect better performances with the DLP4500NIR
2. The easiest way for using the DLP4500NIR for projection is to get a LightCrafter 4500 and replacing the DLP4500 with the NIR one? There are other ways you can suggest? For example, do I have a way of using the DLP LightCrafter related with the DLP3000, to control the DLP4500NIR?
Thank you very much!
Luca