Hello,
I would like to use the DLP LightCommander for a microscopy application. Is there a technical reference describing the optical train/light path inside the device? If there is none available, is there a contact point for this, and would it be possible to describe it briefly?
I am also wondering what the dissipation properties are for the lenses and micro-mirrors - would they be able to withstand 400-700nm light in the 50-100mW/ per millimiter-square range for long periods of time? I am also wondering if it is possible to give specifications for the illumination module (IR/RGB), since I will need to introduce a fiber-coupled source and compatible optics. If there are dichroic mirrors in the light path, what are their specs, and are they switchable or removable?
Thanks very much for your input.
David