Hello,
I have a question from our cusomer.
(Problem)
The pattern projected before appears as an afterimage in the pattern to project.
・The lighting start of LED and the exposure start of a camera are operated
from the external using an input trigger of DLPC200.
(PORT1_Trig_in and PORT2_Trig_in)
・External hardware trigger
・Start of the trigger of these two is the same timing
・Pattern Sequence Mode
(Question)
Is it necessary to delay the start of exposure of the camera?
Should I delay how long the exposure start from the LED lighting start?
Best regards,
Seishin