I did some experiments with LCR and meat with some questions.
1.I remove the entire light engine,and illuminate the DMD with laser beam(showed below pic).
I choose internal test pattern, "Fine Checker Board" . The pattern DMD projects is like this
Every small speckle in the picture is just "Fine Checker Board", but it repeats spatially and periodically, as showed above picture.
Here comes my question. Why the small "Fine Checker Board" pattern repeats spatially? Because there is only one DMD array ,and thus there should be only one spot. I am wondering if it is caused by the mirror covering over the DMD array. If it is for this reason, what's the function of the Plano-convex Spherical lenses next to DMD? With this lens ,the mentioned repetition disappears. By the way, do anybody know the focal length of the lens?
(via PedroGelabert )
2. I remove red LED light source only,and relpace it with a laser one(blue and green LED unlighted ) .Showed below.
It works well .As with LED source, the picture it shows is just the picture loaded . The only difference is the laser projected picture shows small spots arranged neatly , both horizontally and vertically. I guess it is the fly-eye lens. But Why LED picture shows no such spots?
3. The images LCR projects change size with distance.I am attempting to collimate the beam (I hope the image it projects does not change size with distance), do anyone have experiences ?
Thanks
Jin