Hi TI team,
Can anyone tell me if the DLP Lightcrafter camera module could support the Leopard LI-2M01CM and LI-2M05CM. Moreover, Can anyone show me the schematic diagram of system board?
Thanks
Bojing
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Bojing,
Please refer to the discussion about supported camera modules in this thread http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/850/t/321948.aspx
Here the link for downloading the schematics http://www.ti.com/LCRdesigndoc
Regards,
Sanjeev
Hello Sanjeev,
I just checked the schematics. But the camera socket pin no. and the camera header no. seem not to match each other as the header pin starting from D0 to D9 while the socket pin starting from D2 to D11. Can you explain it a little bit?
bojing
Hi Bojing,
The board is built for 10-bit data path going into the DM365 camera port, if you also look at the datasheet, the 10-bit lines are going into 12-bit camera port (where D0 & D1) are not used, the 10-bit connected to D2-D11.
Similarly on the camera header only the 10-bit data lines taken out, the camera header is matching to the one built by Leopard Imaging LI-VM01CM https://www.leopardimaging.com/LI-VM01CM.html
Regards.,
Sanjeev