Hi,
We recently bought the DLP Lightcrafter Evaluation Module. Our goal is to loop over a sequence of 3 different sinusoidal (8-bit) patterns as quickly as possible, preferably obtaining a rate of 120 Hz per image (so 40 Hz for the sequence of 3 images).
If we want to obtain maximum light input, is it possible to:
1) Project R,G and B at the same time?
2) Replace the R, G or B LED with a white one?
3) Project first R, then G, then B version of the same pattern and record all three of them in succession, yielding a total B/W image? What would be the limit in terms of total (R,G AND B) frame rate?
Basically, what way should we approach this problem (max light output preferred at max speed, sequence of three phase patterns) ?
Thanks in advance,
Sam