Hi,
I just tried to upgrade the firmware as described. The FPGA Firmware Upgrade worked nicely.
For the MSP430 I took the file DLP3000-C300REF-MSP430-v3.0/lcr_msp430_v3.txt from the Software Bundle.
After that it showed that the version of MSP430 was "0.0". I supposed it was just a little display bug and tried to change the IP of the Lightcrafter.
This didn't work, I had to restart the beamer and now it doesn't boot anymore, that means it doesn't pass the booting screen.
A red LED on the lower board is blinking every 5,6 seconds.
Can I fix this, and how?
And what would be the correct way to install the MSP430 Firmware Upgrade, I don't want to destroy more Lightcrafters...
Best, Michael