Hello,
I am designing a coustom board based on the DLPC300 controller. The goal is to progect a static monocromatic patter.
As far as I understand the only way to upload data to the DLPC300 is by using Parallel RGB interface (in eather Parallel RGB 24 bit mode or BT.656 mode).
My questions are:
- Is it the only way to upload a monocromatic pattern to DLPC300?
- How can I generate a video signal from a monocromatic static pattern (just an image)?
- If the pattern does not change, should I provide the video signal to DLPC300 continiously anyway. Or it is saved to the SDRAM and then the last fame is displaed also when there is no input signal?
Many thanks
Alex