So I broke one DLP Lightcrafter 3000 EVM and my ex-colleague broke another one. I think that is really a lot for an EVM. Anyway, I need it so I will buy another one.
Now I have some questions about which one to buy if I want to change:
* Which one has a wider Field of view amongst the DLP Lightcrafter 3000, DLP Lightcrafter 4500, DLP lightcrafter Display 2010 or DLP lighcrafter Display 3010?
* Can I also remove the LEDs from DLP lightcrafter Display 2010 or DLP lighcrafter Display 3010?
* Can I project patterns (as I could do on my DLP Lightcrafter 3000 EVM) using DLP lightcrafter Display 2010 or DLP lighcrafter Display 3010?
Thanks, Pepe