Hello,
I am in need of a DLP chip which is at least 8 mm tall (short side). I would like to know all which fit this criteria, regardless of number of elements (pixels?).
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yusufu,
Please check out these datasheets for the DMDs. Please look at the mechanical section for size details.
DLP4500 (.45 WXGA): http://www.ti.com/lit/ds/symlink/dlp4500.pdf ( 20.7 x 9.1 x 3.3 mm)
DLP2010 ( .2 WVGA): http://www.ti.com/lit/ds/symlink/dlp2010.pdf ( 15.9 x 5.3 x 4 mm)
DLP3010 (.3 720p): http://www.ti.com/lit/ds/symlink/dlp3010.pdf ( 18.2 x 7 x 3.8 mm)
DLP3000 ( .3 WVGA): http://www.ti.com/lit/ds/symlink/dlp3000.pdf (16.6 x 7 x 3.5 mm)
Regards
Anshul