We are starting the simulation of the projector based on DLP4710 (TRP type) and we have some doubts about the understanding of the specs.
There are two variants of our understanding presented below. In both cases simulated Illumination beam is ±17⁰, bottom illumination.
In first case the central ray has the angle of incidence on the DLP plane 24 deg. On-state reflects perpendicularly to DLP plane. In this case the angle between DLP plane and Micromirror plane in On-landed state is 12 degrees.
In second case the central ray has the angle of incidence on the DLP plane 34 deg. On-state reflects perpendicularly to DLP plane. In this case the angle between DLP plane and Micromirror plane in On-landed state is 17 degrees.
Which case is correct?