Other Parts Discussed in Thread: DLP4710, DLPC3479, DLPC350
Hi,
If I set the display resolution to 1920 x 1080 using the command "Write Display Size", and the video input resolution to 1920 x 1080 using the command "Write External Input Image Size" : does each mirror of the DMD corresponds actually to each pixel of my video flow, without the influence of any controller algorithm in between ? ie. perfect mapping of pixel data of the video flow to corresponding mirror of the DMD ?
Thanks